Other Parts Discussed in Thread: PCI1520
We are using the PCI1520 in application that could include the use of 32 and 16bit (ISA) PC Cards in a system running Windows 7(32 bit) OS. The Figure 3-1. "Simplified Block Diagram" in the PCI1520 Data Manual refers to the PCI950 IRQSER Deserializer. It doesn't show a connection to the PCI Bus. However, in Figure 6. "Typical System Installation" of the PCI950 datasheet does without a Interrupt Controller. Please clarify. Is a Interrupt Controller needed? And what will be connected to the PCI Bus in reference to interrupt handling? Thanks.
Chris