Hello
I would like to know recommended register values of DS90UB913Q and DS90UB914Q.
Used Mode: 10bit / 100MHz
Best Regards,
Jumpei
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I would like to know recommended register values of DS90UB913Q and DS90UB914Q.
Used Mode: 10bit / 100MHz
Best Regards,
Jumpei
Hi Jumpei,
Could you elaborate on the requirements of your application? 10-bit, 100MHz mode is set from the external MODE pins on the UB913 and UB914 devices. Other features, including bidirectional I2C communication, are set from internal registers.
A block diagram or schematic is always helpful. Thanks!
Dear Ryan,
Thank you for the your answer.
I would like to know about ALIAS ID, SLAVE ID and SLAVE ALIAS ID.
Do these differ from an I2C address?
I don't understand to set what value to these.
Best Regards,
Jumpei
Hi Jumpei,
These fields describe the I2C address of any remote I2C slaves attached to the serializer or deserializer. For more detailed information on these features, see the following app note: