Hello,
We are using the XIO2000a PCIe to PCI Bridge for many years.
Now we discovered that when the XIO2000a receives a message Set_Slot_Power_limit of 0 Watt it starts sending PM_PME messages to the root complex every 100ms and after 30sec the whole communication stops. My understanding is that the XIO2000a should not send PM_PME messages in this case as it is programmed to ignore slot power limit in the POWER_OVRD register (reg. D4h bits 20-22 = 000b). I also verified that the PME\ pin has a pull-up.
Could you please help to resolve this?
Best regards,
Viktor