Hi,
according to http://www.ti.com/lit/ds/symlink/sn65hvs885.pdf Figure(18) an ISO7241 is used to isolate the SPI Pins. In Figure(19) a ISO7242 is used because CE got grounded and HOT (Temp. warning Flag) is a new input.
Why CE is got pulled down? I though its necessary to communicate?
What for an application design should I use now ? Figure 18 or Figure 19 ? I want to cascade 3x HVS885 for our new PLC Input extension card.
Is it right that If I use the ISO742x I dont need optocouplers on each input because the whole input part is isolated through it?!
Kind regards
Ersan