Other Parts Discussed in Thread: DS26LS31C, TPD1E10B09, TPD2E007, TPD4E05U06
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DS26LS31C, TPD1E10B09, TPD2E007, TPD4E05U06
Asaka-San,
Your selection, TPD2E007, should work fine. I looked at the data sheets for these two devices. DS26LS31C is guaranteed using 30pF load(other than Tlz and Thz) Meanwhile TPD2E007 has 15pF load max so i think you should be able to use these two devices together.
Regards,,nasser
Greetings Asaka-San,
Sure the lower the Capacitance the better it would be. This is because the lower Capacitance has less parasitics and less effect on the AC performance of the device. So it all depends on the AC performance(i.e rise/fall time and data rate) of the device. When you increase the Capacitance we are attenuating the high frequency content of the signal. In higher data rates we need to preserve the high energy content to help the receiver on the other side.
Regards,,nasser