Other Parts Discussed in Thread: LMH0034, LMH0394, LMH0344, LMH0384
Hello,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LMH0034, LMH0394, LMH0344, LMH0384
Hello,
Asaka-san
The GS1524 is an older design of an HD (High Definition) cable equalizer. The closest comparable product from TI would be the LMH0034. The two devices are pin compatible, use the same power supply voltage and have comparable AC specs (both are specified to support up to 200m of cable).
The LMH0034 has an advantage in lower power dissipation, (207mW typ vs 264mW), and is guaranteed over a broader temperature range (0-85C vs 0-70C).
If this is for a new design, TI offers a range of newer equalizer designs, including the LMH0344, LMH0384 and LMH0394 which have even better performance and lower power dissipation, but are in a different (smaller) package.
Mark Sauerwald