Other Parts Discussed in Thread: DS64BR401
Hi,
We have obtained customer requests.
Is it not problem to swap the wiring by the convenience of the layout as follows(Proposal1, Proposal2)?
We swap the certain differential input/output channels.
Is there something affect on the performance?
(a) Proposal1
Input signals and output signals of Ch0 and Ch2 were connect normally,
Input signals of Ch1 and Ch3 are swapped(output signals are inverted in RX-IC).
TX-IC DS64BR401 RX-IC
[Ch0] Cs Cs
TX0(+)----||--IB0(+)--OB0(+)---||---RX0(+)--|Differential to Single Converter
TX0(-)----||--IB0(-)--OB0(-)---||---RX0(-)--|
[Ch1] Cs Cs
TX1(+)----||--IB1(-)--OB1(-)---||---RX1(-)--|Differential to Single Converter + Inverter
TX1(-)----||--IB1(+)--OB1(+)---||---RX1(+)--|
[Ch2] Cs Cs
TX2(+)----||--IB2(+)--OB2(+)---||---RX2(+)--|Differential to Single Converter
TX2(-)----||--IB2(-)--OB2(-)---||---RX2(-)--|
[Ch3] Cs Cs
TX3(+)----||--IB3(-)--OB3(-)---||---RX3(-)--|Differential to Single Converter + Inverter
TX3(-)----||--IB3(+)--OB3(+)---||---RX3(+)--|
(b) Proposal2
Input signals and output signals of Ch0 and Ch2 were connect normally,
Input signals and internal singals of Ch1 and Ch3 are swapped.
TX-IC DS64BR401 RX-IC
[Ch0] Cs Cs
TX0(+)----||--IB0(+)--OB0(+)---||---RX0(+)--|Differential to Single Converter
TX0(-)----||--IB0(-)--OB0(-)---||---RX0(-)--|
[Ch1] Cs Cs
TX1(+)----||--IB1(-)--OB1(+)---||---RX1(+)--|Differential to Single Converter
TX1(-)----||--IB1(+)--OB1(-)---||---RX1(-)--|
[Ch2] Cs Cs
TX2(+)----||--IB2(+)--OB2(+)---||---RX2(+)--|Differential to Single Converter
TX2(-)----||--IB2(-)--OB2(-)---||---RX2(-)--|
[Ch3] Cs Cs
TX3(+)----||--IB3(-)--OB3(+)---||---RX3(+)--|Differential to Single Converter
TX3(-)----||--IB3(+)--OB3(-)---||---RX3(-)--|
We think that our proposal1 is not problem, but the proposal2 is problem.
Please tell us about it.
Best Regards,
Kato