Other Parts Discussed in Thread: LMH0302, LMH0384, LMH0307, LMH0303, LMH0344, DS25CP104A
Hello,
I'm using your LMH0384 as my cable driver,the source of the SDI is a lattice's FPGA and the destination is a LMH0302. I use the pin mode of LMH0384 on my PCB and so do the LMH0302.
I've tested the destination of LMH0302 before,It worked pretty good whatever feed it with a 1.485G or 2.97G SDI signal.
Now I want to talk about the source.They work very well When I pass a 1.485Gbps SDI signal from LMH0384 to LMH0302 with a coaxial cable,But they're down when pass a 2.97G SDI signal.Then I try to adjust the signal's VPP and others conditions,but it looks like dead.
I want to know the LMH0384 will rebuilt the passed signal, or not?I don't have a machine to check the eye of the signal,,,I block the diff-signals with ground on the PCB,the distance from FPGA's pin to LMH0384 is about 7cm,and AC coupled.Would you please give me some suggestions?
Many thanks
Tom