Other Parts Discussed in Thread: TPD4S012
Hello TI Engineers and company,
I would like a clarification on a devices that you offer for ESD System level protection; e.g., TPD4S012. The target application is a portable DAQ for medical instrumentation and it will, of course, some with an USB interface to be connected to a computer.
What has sparked a heated debate here is the use of these devices to ensure our system meets 15kV air discharge/contact ESD ratings as one level spelled out in the IEC61000 4-2. Although we have not investigated it at this time we do know that there are specially rated connectors, from Spectrum Control, that integrate ESD protection and are rated for 15kV air/contact. The rub of course is cost and availability of USB type connectors.
How can the TPD4S012 and other similar devices from TI as well as your competitors claim IEC 61000 compliance when it is a system level standard and not a component standard as is covered by JEDEC? I am by no means an ESD expert, but the reading I have done so far implies that rating an intergrated circuit to the IEC 61000 system test is dubious. I have also heard (nothing in print) that different systems; i.e., board layout, is the big unknown in repeatability for component testing to meet IEC 61000. One system will pass while the other may fail. I have posed this question to several of your competitors and received nebulous responses in return.
The real question is this: Since you claim IEC 61000 compliance on your device even though it is a system level test, then do you test the component in accordance to the IEC 61000 setup in a generic system and rate the device accordingly?
Thank you in advance for your sage advice.
-Ken