Other Parts Discussed in Thread: AM26LV32E-EP
Hello,
I am looking to use the AM26LV32E-EP and I wanted to know what is the worst case max switching frequency for the full military temperature range. The datasheet states that it is specified for -55 to +125C operation, but the only max operating frequency is 32MHz which is typical with a Ta=25C. What is the maximum worst case moperating frequency from -55 to +125C. Is there a curve available or just a guaranteed minumum for both extremes?
Thanks.