Other Parts Discussed in Thread: DS90CR288A, DS90CR287, DS90CR285
In a customer's circuit design (Defence Engineering Corp.), they are using the National parts DS90CR288A and DS90CR287. They are also using the Linear part LTC6995-1 to enable the DS90CR287 through the PWR_DWN(active low) pin. The DS90CR288A provides the input data and clock to the DS90CR287. The data and clock output from the 288A National chip looks good, and the enable provided from the 6995-1 looks correct (the delay is in the 30 micro-second range). The National 288 chip powers up when power is applied to the circuit and it has data immediately for decoding. The National 287 chip uses the 6995-1 to delay its PLL initialization until a time after the National 288 chip is providing a stable clock, and this has been verified. However, there is no output from the National 287 chip.
Can you think of any reason that would cause the output to not function? I currently am having them double check their communicaiton with the PWR_DWN pin. Thanks!