Other Parts Discussed in Thread: ADS5281
Hello,
I wanted to convert the LVDS ouput of ADS5281 to LVTTL/cmos .So I decided to go with high speed differential line receivers..
But speed of ADS5281 which i am going to use in my project 50 Msps 12bits/pulse so 12 x 50 = 600 Mbps ..so i need the receiver which accepts the signalling rate above 600Mbps...so I went through through dis link to make a search http://focus.ti.com/paramsearch/docs/parametricsearch.tsp?family=analog&familyId=736&uiTemplateId=NODE_STRY_PGE_T ..so interestingly i found few receivers like
but when i opened the pdf file http://www.ti.com/lit/ds/symlink/sn65lvds388a.pdf... it is showing upto 200Mbps..I need 600mbps ..i searched a lot but it is showing on the page but not in the pdf file ...can anyone help on this?/ is dere alternative to interface to ads5281 which has 50Msps?? i wanted to convert lvds ouput to single ended /lvttl/cmos output