Other Parts Discussed in Thread: TUSB7340
Hello. I have big problems with my Silverstone EC04 USB3 card (TUSB7340) and music synthesizer Access Virus TI2. When I plug Virus TI2 into USB3 card port I have a BSOD, also Windows 7 goes to BSOD during boot up if Virus TI2 connected to Silverstone EC04. With on-board USB3 Hostchip (ASMedia 104x) my Virus TI2 works fine.
The Support of the Access Music says this "As I mentioned already in my earlier email the BSOD is not just caused by our driver, but also the drivers for this PCI card, so this is definitely something you need to get in touch with the manufacturer, especially if the Virus works fine on an on-board USB port". Drivers for TUSB7340 was taken on this site and up to date, v. 1.16.2.0.
Minidumps of BSOD is here: http://www.sendspace.com/file/7nuv1t
Please, help me.