Other Parts Discussed in Thread: TUSB3410
I'm looking on advice for TUSB3410 COM port problem.
We're a canadian bank and in a Virtual Desktop migration project. The PC are replaced by Samsung Zero Client "terminals". These terminal include a builtin com port which is in fact a TUSB3410. Unfortunatly for us samsung has just started shipping the particular model of zero client (NB-NH) with the TUSB3410. Until last week the USB/COM port was a prolific... and right when we go production they switched the hardware on us. All of our testing was done with Prolific. The only place I could find a Windows 7 32 driver for the TUSB3410 is here. I downloaded it from the 3410 page. It installs fine, the driver and device seems healthy (COM number is ok) but the particular device we need the COM port for just does not work with the TUSB3410. If I switch to a terminal with a prolific chip it works. If I use a FTDI USB/COM converter it works right off the bat.
I'm not sure if the Windows 6.7.2.0 driver I download from TI is a generic driver that whould work with any implementation or if I absolutly need a Samsung specific driver.
Our application is an inhouse application that prints bank statements on a serial IBM Passbook printer (the windows printer driver is a inhouse serial driver) so we will put our programmers on the issue. But that same print driver works just fine with Prolific and FTDI so I'm assuming it's ok.
We are trying to dig though our Samsung contacts the help us resolve the issue but at the same I'm coming here to see anybody has insight or advice.
Thanks in advance.
Eric