Other Parts Discussed in Thread: TPD2E007, TPD2E001
Customer is using the TP3420A device. The TP3420A Line Interface Circuit Considerations Application Note (Section F on page 7) references two parts that are obsolete. TISP2180 from TI and P1553AA from Littlefuse. Customer looking at the P3100SCLRP from Littlefuse as replacement. Is there a better recommendation?
Customer is using the ISDN in TEM (TE Master) mode. If he picks format 1, can he still change the clock frequency? On the datasheet table 3 says it is fixed depending on the format he picks. On page 14 of the datasheet commands BCLK1n to BCLK4n allow him to change them. Which is correct?