Other Parts Discussed in Thread: ISO1050
Hey,
i have a big problem with the CAN but only with the PIC18F2xk80 and the ISO1050. The CODE and the settings are ok, they works on me testboard with a conection to the CAN Demoboard for the 18F or when i youse a MCP2551 as Transiver. But when i change this CAN Transiver to a TI ISO 1050 it dosent works. I need the isolation of the other part.
When i youse a dsPIC30F4012 in the same Layout the circut with the CAN works....
The TX Chanel is the problem, the flags are not ok. When i conectet a MCP2551 (onlyTX and RX in not CAN) on the same PIC togehter with an ISO1050 the ISO1050 works on the CAN side!
whats happen??? have same body anny idaers?
Thanks for help
Thorsten