Hello TI Team & Community,
I am using one TUSB2046B hub controller to talk to two other TUSB2046B hub controllers in order to create a total of 10 downstream ports. I am, in effect, creating a 10-port self-powered hub. I have reviewed the device datasheet, as well as the two reference schematics (motherboard implementation + self-powered implementation.) I have also reviewed a number of the posts in this forum regarding this device.
I recognize that the schematic shown in the device datasheet is not a complete product schematic, and that you refer to the two reference schematics. I do wonder about what looks like external "de-glitching" on the overcurrent signals between the TPS2044 power switch and the TUSB2046B hub controller as shown in the self-powered hub reference schematic. The datasheet for the TPS2044 says that the /OC outputs are already de-glitched, providing 4 to 15 ms of delay. Do I need to use the external RC nets, or can I reliably rely on the TPS2044 internal deglitching?
I have noted a number of threads discussing the required reset timing. On the self-powered hub reference schematic, note 3 refers to a DS1233 reset IC - which doesn't seem to be present anywhere (?) I see a 22 ohm resistor to 3.3V and a 100nF capacitor to ground on the reset - surely these values are not correct. I have seen other values mentioned in the previous threads, and it seems that a 15k pull-up and a 1uF cap is correct - yes?
I am not sure about the purpose of the 2N3904 transistor circuit on the self-powered hub schematic. It appears to be switched by the upstream VBUS, but beyond that, I don't understand what it is doing with the pull-up resistor R191 to DP, or why its collector is connected to the /RESET on the TUSB2046B and the CS on the EEPROM. Can you please explain what is going on with all of this?
I also welcome any suggestions you might have regarding what I am attempting to do. Thank you in advance for your assistance!