Other Parts Discussed in Thread: SN65LVDT388
Hi,
I am looking for a LVSD receiver that is able to receive 8 bit lvds signal generated by FPGA, after this LVDS Receiver, the 8 bit signal is used as switching signal to control 8 switches of my application. the signal rate of it should be around 200MHz to 400 M Hz
I am thinking SN65LVDT388, but since it is a simple buffer and does not have the clock input, I am afraid of the output signals of this receiver are not synchronized due to the output skew and wiring issues.
so my questions are:
1. Do you have any product that can do the work described above, and synchronize the output signals as well? and how do I use it?
2. How do I connect the receiver with the FPGA? does copper wire work? or I have to use some special cables?If so, what's the part no.
Thanks in advance!