Other Parts Discussed in Thread: DP83848I
I have an issue that hopefully someone can help me out with. I have a DP83848I chip connected to an ARM STM32F407. Everything works fine until I turn off my circuit with the ethernet cable still plugged in. After about 30 seconds the link light on the switches shows a link and the port starts getting hammered with sent bytes.
I have tried 2 different gigabit switches Asus and Netgear and both do the same thing. The netgear is a prosafe + so I was able to connect and see that the port gets flooded with sent bytes. Also what happens is the other ports get taken down because the switch gets overloaded.
I then tried 2 other switches 10/100 and everything works normal. No link light when my board is turned off and no flooding of the port.
Any idea what might be happening or what I should be looking for.
Thanks