Hi,
I want to use for a new design a TLK2711-SP (SMD 5962-0522101VXC) with a serial speed of 2 Gbps.
I would like to know what is the best nominal value for the supply voltage VDD for a speed of 2 Gbps because it 's not clear in the datasheet.
In the TLK271-SP datasheet :
VDD supply voltage frequency range 1.6 Gbps to 2 Gbps : 2.5 V NOM
VDD supply voltage frequency range 1.6 Gbps to 2.5 Gbps : 2.6 V NOM
In the 5962-0522101VXC datasheet :
VDD supply voltage frequency range 1.6 Gbps to 2 Gbps : 2.375 V dc to 2.7 V dc
VDD supply voltage frequency range 2 Gbps to 2.5 Gbps : 2.5 V dc to 2.7 V dc
Regards