Other Parts Discussed in Thread: TUSB3410, TUSB6250
I've been trying to load firmware from PC to TUSB3210KBD-REV 3 EVM using the Apploader but haven't see success so far.
The OS on my PC is Windows XP (32-bit). The EEPROM has been removed from the socket, and the jumper positions on the EVM are:
- U3: 2-3
- U9: 1-2
- U12: 1-2
I download the software "TI Apploader Driver (Rev. A)". The EVM is unplugged during the installation process. After the TI USB Application Loader Driver Wrapper is installed, I follow the instruction modifying the Apploader.INF to specify the binary file to be TUSB2136.BIN in all three places, then copying Apploader.INF, ApLoader.SYS, and TUSB236.BIN into a new folder C:\Apploader. When the EVM is plugged, it is detected and listed under "Other Devices" by Device Manager. The VID and PID can been seen under device details as "USB\VID_0451&PID_0040\5&57CA357&0&1". But when I try to install the device driver by directing it to C:\Apploader, the Hardware Install Wizard shows that "Cannot Install this Hardware" because "it cannot find the necessary software". I have tried this process multiple times without success yet not knowing why.
Can someone help me? Thanks!