Other Parts Discussed in Thread: DP83848YB
Hello TI Technical Support,
I writing a test program to test the DP83848YB device using a Credence digital component test system. I do not have the DP83848YB connected to an Ethernet host so I am attempting to perform the internal Loopback function to verify the signal path between TXD[3-0] and RXD[3-0] through the device. I set bits 14 and 8 of the BMCR (Loopback enabled, 10MPS, at full duplex) and the remaining bits to 0. I write the Preamble pattern to TXD[3-0] then a start of frame followed by a fixed data pattern. I am anticipating a similar data pattern on RXD[3-0] and just read all zeros. What else needs to be done to use the loopback feature for this device?
Thanks,
Mark