This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO5500 - Fault pin continuously becoming damaged

I have been using iso5500 for my power designs. Issue faced is with the fault \ pin. we are having a power board separate, controller board separate kind of design. The faults are all wired and 'or'ed to the controller fault pin. Each ISO5500 fault pins are pulled up with 4K7 resistors to 5V supply very near to them. The power board is a Full H McMurray Bridge. A 470PF capacitor is also connected to ground from each of the fault\ pins to its immediate input ground pin. Thinking of ESD issues, a transient voltage suppressor P6KE6.8A is also provided very near to each of the fault\ pins with their respecive immediate ground points. However the 'or'ing of all fault\ pins are via track running around the board which may have a length of a total of 12-13 inches since its a power board. The 'or'ed fault connection is taken to the controller board through an external wire connection.

Now coming to the problem, The fault\pins are getting shorted and the system gets tripped down as the controller sees a low in its sense pin. While checking either of the 4 fault\ pins of the bridge is found to be permanently pulled low. However the iso5500 ic seems to be working in all respects with the output fault circuitry is working fine even though the fault\ pin is in the pulled down/shorted condition. The system is about to go for production and all our designs have been stalled because of the same issue. If the issue is not sorted out immediately then we would be forced to shift to some other gate drivers. Please help in this regard. TVS helped us in lowering failure counts although not fully solved the issue. P6KE6.8A is capable of snubbing the transients greater than 5.75V as per the data sheet.