This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UR916 ibis model error



Hi

I am doing a high speed design with the DS90UR916 and is experiencing some error with the ibis model in the simulation.

  • while performing a driver analysis on the PCLK pin, there is a strange signal at the rising edge, which after checking with ibis syntax checker, warning of data is non-monotonic. Is there anyway of resolving this?
  • pin 49/50 is NC and cannot be simulated. Is it possible to simulate the LVDS signals since now the RIN+/RIN- are not possible to be import in.


am also attaching the screen shot of the signal of PCLK as follows:

4621.waveform.tif


Regards

Lin Biao