Other Parts Discussed in Thread: DP83848I-MAU-EK
Hi all,
I used DP83848VVVBC which is sample requested from TI. I had four PCB board prototype which were populated with DP83848VVVBC as the ethernet physical chip. The MCU that I used is PIC32MX675F512H with Microchip TCP/IP stack.
All the board were functioning at the beginning, but after one day, three of my boards were malfunction. I cannot detected the physical chip so I suspect the chip somehow malfunction, after I replace the DP83848, two of my boards were recovered. I did not go in deep to find out the problem because I think that this might be the soldering problem to cause these boards malfunction.
After two month, one of my board malfunction again and cannot detect the network chip. I doubt is that any design error that cause this to happen.
Here is my schematic and PCB layout file in Altium10. I hope someone can help me out to solve this problem.
Thanks and appreciate anyone to give me advices.
Donnie Lee