Other Parts Discussed in Thread: PCA9517
I have a few questions about quiescent supply currents of this device that are not specified in the datasheet.
1. The drivers of the device are enabled when V_CCA is above 0.8 V and V_CCB is above 2.5V. What are the maximum currents drawn from V_CCA and V_CCB if only one of them is high enough, i.e.:
1a. When V_CCA is above 0.8V but V_CCB is below 2.5V
1b. When V_CCB is above 2.5V bot V_CCA is below 0.8V
2. What are the maximum currents drawn from V_CCA and V_CCB when EN=0?