Other Parts Discussed in Thread: ISO7640FM, ISO7240M, ISO7140FCC
Please see the below url page 39 as Virtex6 LVCMOS 25 DC level.
http://www.xilinx.com/support/documentation/user_guides/ug361.pdf
I introduced ISO7240M, ISO7640FM and ISO7140FCC to our customer then our customer has some questions.
Could you please kindly let me know about below questions?
I think that ISO7240M can't use for Virtex6 LVCMOS25 I/Odue to VIH(min) is 0.7*Vcc.
ISO7240M Vcc(min) is 3.3V.
But, ISO7640FM and ISO7140FCC can use for Virtex6 LVCMOS25 I/O due to these device's VIH(min) is 2.0V
(2)
Our customer use below two Vcc conditions.
But there is not electrical characteristics.
<a>Vcc1=2.7V、Vcc2=5.0V
<b>Vcc1=5.0V、Vcc2=2.7V
If yes, should we refer which electrical characteristics?
Best Regards,
Ryuji Asaka