Other Parts Discussed in Thread: OMAPL138
Hi,
I'm working on an application that interfaces the DP83848 (Ethernet PHY) with the OMAPL138 processor. At this point we got the OMAPL138 to detect the Ethernet PHY and I'm able to read and write to its register but I haven't being able to link or get the autonegotiation to be completed. I'm monitoring the OMAPL138 MDIO LINK register to look for any linking signs plus looking at some of the DP83848 registers as well. Here are a few of the values that I'm currently getting on the DP83848 side:
BMCR = 0x3100; Good
BMSR = 0x7849; Not Good, no link
ANAR = 0x0181
ANLPAR = 0x0000
ANER = 0x0004
PHYIDR1 = 0x2000; Good
PHYIDR2 = 0x5C90; Good
ANER = 0x0004
Also, I'm trying to connect from our board design to a NetGear Switch and from the switch to a PC. The idea is to perform a test to send packets via ethernet from the OMAP application to the PC. We are also using the lwip library provided with the Starterware drivers. We are currently troubleshooting but so far haven't find out the actual reason for not linking. Please provide any pointers if someone is familiar with a similar error and/or if additional information is needed to understand the problem.