Other Parts Discussed in Thread: DS100MB203
Hi,
Our customer uses DS100MB203 on their system board.
Question)
Could you please tell us how you should set "MODE" pin or register 0x17 bit6 for CPRI (9.8304 / 4.9152 / 2.4576 Gbps) ?
I think you should set to PCI Gen1/2, 10GbE mode as below, am I correct ?
Pin mode : MODE pin = 0 : Pull down to GND through 1k Ohm resistor
SMBus mode : Register 0x17 bit6 = "1"
Best Regards,
Kawai