Other Parts Discussed in Thread: TPL9202
I know generic comparisons can be dicey...but that's what I'm looking for, just the same. ;)
Assuming a 41 C ambient, all 8 outputs ON, low-side switching 12V relays, which device can handle more relays per output?
At a glance, the ULN2803 seems more capable, throwing around numbers like 500mA continuous (abs max, I know), where the TPL9202 pretty solidly says "150 mA". But when I start running numbers on power dissipation, the ULN2803 seems to come up at about half that of the TPL9202...which at a gut level isn't that surprising given the thermal pads on the TPL9202. Assume we use a multilayer board and the recommended layouts.
John