Other Parts Discussed in Thread: STRIKE
- Hello,
I would like to ask you about the ISO7231.
I tested the device as below Test Conditions
1. Test Conditions
1.1 Pulse Waveform: 1) Pulse width=1uS, 2) Cycle=16mS, 3) Period: 5 ~10 Minutes, 4) Amplitude: 2kV
1.2 Adding Point: GND
2. Result
2.1 EN pin is connected to Vcc : Current Consumption is being increased up to 100mA and the device is stuck.
2.2 EN pin is open, the device is normal operated though adding the Waveform signal continually.
My question about these results, Why the operating is more stable when EN pin is Open?
Is the EN pin Open more stable than EN connected to VCC?
Please give me the stucture of EN pin internally because I need to review ESD for En terminal.
Finally, Why current of VCC connected to EN is increased?
Thanks and Best Regards