Hi, please let me confirm how to use loopback function.
In SMBus mode, loopback setting is controled using register 0x07[1:0].
Is register 0x07 [1:0] only can be used in the following setting ?
Register 0x07 [1:0] = 0x0 : INA to OUTA, INB to OUTB
Register 0x07 [1:0] = 0x3 : INA to OUTB, INB to OUTA
What happens when this is set to 0x1 or 0x2 ?