Dear All,
I'd like to use the ISO7242 to isolate the UART from the RS485 transceiver (TX->INA, RTS->INB, RX->OUTC and CTS->OUTD).
In TI application notes, I found that is suggest to use ISO71XX for this application.
In the ISO71XX's datasheet is also specified in the applications section.
Are there any problem in my setup?
The last question is about the isolation rating.
In the ISO71XX's datasheet is indicated that the isolation value is: 2500Vrms but the same parameter there isn't in the ISO72XX's datasheet.
Could you tell me How much is this value, please?
Thanks a lot.
Best regards.