Other Parts Discussed in Thread: LMH0002, SN65LVDS104, LMH0344, DS90CP22, LMH0395, LMH0044
Dear Sir, We want to receive a 270Mbps DVB_ASI stream driven by a LMH0002,
and fanout to two output. Since the cable is very short (less than 10cm), we are
considering to use a SN65LVDS104 to receive the signal directly and not use any
equalizer, will it be possible?
Another question is: In LMH0344 circuit, there is a 6.8nH inductor parallel with a
75ohm resistor in the receiving circuit, what is the purpose?
Thanks for help,
Tang