Other Parts Discussed in Thread: DS110DF410
Hi Team,
When the input is connected at the same time (same signal), what is the maximum channel to channel skew of DS110DF410 ?
Best Regards,
Kawai
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DS110DF410
Hi Team,
When the input is connected at the same time (same signal), what is the maximum channel to channel skew of DS110DF410 ?
Best Regards,
Kawai
Hello Kawai,
The intra-pair skew (i.e. between TXP and TXN for any output) is about 3 ps. The skew between two channels, for example between channel 0 and channel 1, is not a specified/tested parameter. Note that the propagation delay (a.k.a. latency) through the device from input to output at 10.3125 Gbps is about 300 ps. I expect the skew between two channels to be much less than the propagation delay through a channel, and more on the order of the intra-pair skew (few picoseconds). However, I should stress that this is not a tested or specified parameter. Hope this helps.
Best regards,
Casey Morrison