Other Parts Discussed in Thread: SN65LVELT23
Hi,
I am currently designing a circuit in which I get a Single ended LVPECL output signal from a device which I need to convert to single ended LVTLL signal.
The device from which I am getting a single ended LVPECL signal is AFBR5803 (pin4)
The single ended LVTTL signal I will give to an FPGA.
For the same I intend to use SN65LVELT23.
But nowhere in the datasheet it is mentioned that the SN65LVELT23 can accept single ended input, everywhere it is mentioned as differential inputs. I wanted to know whether the device can accept single ended input? If yes can you please mention the required interface for the same.
Else can you provide me an alternate solution to this problem.
Thanks Regards
Raquib Akolawala