Other Parts Discussed in Thread: SN65LV1224B, SN65LV1023A, TLK1501, SN65LVDS301
Hi
A medical customer has a 2 mega-pizel video camera with 10bit output at 30 frames-per-second. (Output may be 12-bit, but more likely to be 10-bit.)
He needs to serialize this and transmit over either a twisted Copper pair in as low a power way as possible, as his device runs off a LiPoly rechargable. So the receiver power also matters. The communication is one-way, from the camera up the cable to a receiver.
I have had a look at our serializers and power consumed seems high at such a high data-rate. Transmission distance is cm, say 100cm.
Can you suggest what would be our lowest-power method to do this?