Other Parts Discussed in Thread: TLK110
Hello,
The TLK110 is not able to establish link after auto nego funection(set bit 12 = 1 (auto-neg enable) and bit 9 = 1 (restart auto neg) in BMCR register).
However, a valid link (10MBaseT) established successfully while preform a forced modes and run a MII loopback test.
Is that any clue how to address the auto nego fail issue.
One thing may be related, the pin LED_SPEED/AN_1 is not connected(NC), and the LED_LINK/AN_0 pin and the LED_ACT/AN_EN pin connect to corresponding LED only( no 2.2k resistor connect to GND or VCC ).
Thanks you,
Elvis