Other Parts Discussed in Thread: ISO3086
Does the ISO3086 transceiver require biasing on the Rx input?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ISO3086
Does the ISO3086 transceiver require biasing on the Rx input?
Hi Trevor,
The R pin is actually an output pin. The D pin is the input data pin. Neither require biasing, as they are CMOS (not open-drain). Does that answer your question?
Thanks,
Jason Blackman
Hi Jason
I meant on the receive differential inputs A and B as the datasheet refers to it as having a failsafe receiver
Regards
Trevor
Hi Trevor,
It depends on your application, but under normal circumstances failsafe resistors are not required on the A and B lines.
What the datasheet is referring to about the failsafe receiver is that the receiver threshold values are intentionally biased to be negative. Normally with RS-485, -200mV and below is a low while +200mV and above is a high. That case requires failsafe resistors to ensure that the receiver is in a known state during open, short, and idle conditions where the differential voltage is normally 0mV.
The ISO3086 (and many of our other transceivers) will be in a known state when there is greater than -10mV between A and B. That covers open, short, and idle. If your system is very noisy, then additional failsafe resistors may be required because you can't be sure where the receiver is going to transition in between -10mV and -200mV.
Does this help to explain the functionality?
Thanks,
Jason Blackman