Other Parts Discussed in Thread: DP83848I
Dear all:
I am using DP83848I's SNI interface. But I have met a problem of TCP re-transmission when using that port.
The MII_MODE pin is tied to high through a resistor and the SNI_MODE is also tied to high through a ressitor.
The BCMR is set to 0x0000 and the ANAR is set to 0x0021.
If I pull down the Ethernet line and then plug in it. The communication will be OK. If I set the PC as 10M-Half Duplex, the communication is also good.
Can any one give me some hint?