Other Parts Discussed in Thread: SN65LVDS315
I am using the TI SN65LVDS315 Parallel to MIPI CSI 1 converter with a VGA format Omnivision sensor.
At the receiving end I am using a Toshibs CSI to Parallel (bi directional ) bridge chip to convert back to Parallel. This is purely for design verification purposes.
The Toshiba chip specifies CSI2 input and I cannot find any information relating to backwards compatibility between CSI 2 and CSI1. It seems that CSI 2 supports between 1 and 4 data lines, as opposed to only 1 for CSI 1.
Can anyone tell me if there are any reasons why a CSI 1 device will not work with CSI2.