Other Parts Discussed in Thread: DS42MB100, DS90UH925Q, TFP401A
Dear all,
I have to create a multiplexer for an LCD display with an FPD-LinkIII input. The device is using a DS90UH925Q and a DS90UH926Q combination to transmit the RGB data. I planed to use a DVI Input, change the data format with a TFP401A into RGB and create a second data stream with a second DS90UH925Q (is the DS90UB925Q also possible?). Then I will use a DS42MB100 as a multiplexer for my CML bit streams. Can I use this IC for this application?? If yes do I need the AC coupling capacitors into the new short lane too?
Best regards
Thomas Titzmann