Other Parts Discussed in Thread: SN65LVCP114
We are testing SN65LVCP114 in a SFP+ application.
On the board, the trace length between SFP+ socket to LVCP114 PortC is less than 2 inches. From LVCP114 PortA to 10G PHY(not KR capable) is another 2 inches. The PortB of LVCP114 is connected from IN back to OUT with about 2 inches trace without cap. LVCP114 is operate at 2.5V and the ripple is <8mv with dedicated regulator.
Our first test case is that we loopback on Port C and test BER. So the 10.3125G XFI goes in CIN and loopback out COUT. The setting is: EQ=1.3dB, Gain=0.5, VOD=0.6. We are observing bit error at the rate of 10E-12 with DAC cable. And if we use SFP+ optics module, the bit error rate is much higher at 10E-10 (barely working).
Now for the same board, if we bypass the LVCP114 and connect trace from SFP+ socket to PHY directly (we have backup traces, breakers on board to characterize the design), the bit error rate is 0 after 8 hours of running.
The second test is that we enable DIAG=1, and select PortB, since PortB IN and OUT are connected, so the signal is loopback through port B. This time, we have much worse BER. DAC cable is at 10E-11, and SFP+ optical module does not work.
We are wondering if the LVCP114 is designed for such application and appreciate your insight.