Other Parts Discussed in Thread: CDC7005
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CDC7005
Hello,
Those parameter are not typically specified on an oscillator input, it is the threshold level which is specified instead, in this case XI has a threshold level equal to one half of the voltage measured on PLLVDD_core; if PLLVDD_core is 1.8V the threshold level of XI will be 0.8V.
You can find an application note for crystal selection at the below link.
Regards.
http://e2e.ti.com/support/applications/high_reliability/f/30/p/165912/608498.aspx
Hello Elias san,
I'm sorry for my postiing again and again.
We can't have any XI input information without below?
Then , I will explain to our customer it. Thus, please kindly let me know above my understanding is correct or not.
http://e2e.ti.com/support/applications/high_reliability/f/30/p/165912/608498.aspx
Best Regards,
Ryuji Asaka