I would like to do some pin swapping on the . TI’s EVM apparently uses the connector on output side, but I want to put it on input side so the P’s and n’s are reversed on both sides of part. Lane 0-3 will be reversed as well. This product is only passing the data through, and is not interpreting anything.
Also, the link training is done from source side. It will be controlled on my side so I will know if it’s lane 0 or 3.
Should be able to be controlled via i2c.
So the question is:
Is there anything specific I need to do for the p vs. n since the part is differential in.
Also…can this be done with LVDS repeaters…Same question?