This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The difference between 75lbc173ad and 75lbc173adg4?

Hi,

What is the difference between 75lbc173ad and 75lbc173adg4?

Thanks
Avi

 

  • Hi Avi,

    The build specification for both the SN75LBC173AD and SN75LBC173ADG4 are actually the exact same. The G4 device is a guarantee that the device is “Green”. This means that it is lead, antimony and bromine free, can be reflowed in a lead free PCB reflow process (260°C exposure), and the lead frame finish is NiPdAu which has an “environmental Category 4” rating. There actually is no need for two package names.

    Let me know if you have any other questions!

    Thanks,

    John