Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSB81BA3E use of internal regulator

Other Parts Discussed in Thread: TSB81BA3E

I want to use the internal regulator of TSB81BA3E. -> VREG_PD will be connected to GND.

I want to separate the DVDD-CORE and the PLLVDD-CORE pins in PCB-Layout.
I want to connect only two banks of KerKos to DVDD-CORE and PLLVDD-CORE pins.
This means on the unassembled PCB the DVDD-CORE and the PLLVDD-CORE pins are galvanically isolated!

Question:
Are there two internal linear regulators, one for DVDD-CORE and one for PLLVDD-CORE or
is there only one regulator and DVDD-CORE and PLLVDD-CORE pins are connected internally or
do I have to connect PLLVDD-CORE via an ferrite bead with DVDD-CORE?

Remark: I read the SLLA153A - October 2004 Application Report for the TSB41BA3A.
In the schematic at PDF page 9, the ferrite bead FB4 on PLLVDD(CORE) make a high frequency isolation from the left sided PLLVDD-Core pins to the right sided attached KerKos.
That does not make sense to me and looks like a mistake in this reference design.

Regards
Andreas