Other Parts Discussed in Thread: TUSB7340
TUSB7340 in Linux 3.0.3.5 system.we use USB3.0 HDD copy test. occur below as error xhci_hcd 0000:01:00.0: WARN: transfer error on endpoint usb 4-3: reset SuperSpeed USB device number 2 using xhci_hcd xhci_hcd 0000:01:00.0: WARN: short transfer on control ep xhci_hcd 0000:01:00.0: xHCI xhci_drop_endpoint called with disabled ep d6ab7120 xhci_hcd 0000:01:00.0: xHCI xhci_drop_endpoint called with disabled ep d6ab714c what next step.
by the way, we check out pin A45, B41 of TUSB7340 connect PCIE port REFCLK+ and REFCLK- it's opposite with TI's TUSB7340EVM layout, may be it important cause of the foult.
thanks