Other Parts Discussed in Thread: DS92LX1621, DS92LX1622
Hi All,
I am a EE grad student at Texas A&M majoring in Analog and Mixed Signal.
I am currently working on a PCB test board for a Time-to-Digital Converter. The Width of my output Digital word is 16 Bits. Due to the large amount data storage required and the limited number of oscilloscope channels available, I have opted to serialize the digital word and use 1 channel of the a high performance oscilloscope in our lab to be able to store all the data in the characterization test. Upon searching i decided on the DS92LX1621 serializer, which meets all the expected requirements. I want to find out a number of things about this part:
1. Is it possible to use this DS92LX1621 in the said configuration without the DS92LX1622 De-Serializer.
2. Are the default Register settings sufficient for the said purpose or do I need to wirte to the DS92LX1621 via the I2C interface (SCL and SDA pins).
3. What should be the logic values for the following pins : MODE, PBD.
4. What should be the RID resistor value if i require it .
5. Do i need to use the GPIO Control interface (GPIO[0] and GPIO[1] pins).
Thank you.
Regards,
Noble Narku-Tetteh