Other Parts Discussed in Thread: LMH0346
Hi,
The Block Diagram in the datasheet shows the differential outputs of the LMH0346 powered by VCCO. The application circuit examples show VCCO connected to a 3.3V supply.
Figure-4 contradicts the Block Diagram and VCCO pin description, and shows the output driver powered by VCC.
Q1. Is the output driver powered by VCCO or VCC?
Q2. Since the outputs are LVPECL compatible, can VCCO be connected to a 2.5V supply (assuming it powers the output driver)?
Q3. Why is the VCCO spec. missing from the DC Electrical Specs.?
Q4. VCMO is spec'ed as VCC-VSDOD. Shouldn't that be VCCO-VSSDOD?
Thank you
Naji